NX Soft Radius Change at End option of [Edge Blend].

2021-10-06T23:26:06Z
NX for Design

Summary


Details

In [Edge Blend] command there is a "Soft Radius Change at End option" in Variable Radius group.
What does it mean?



Solution

"Soft" in this case means the rate of change in the variable radius approaches zero at the end of the edge chain.  Thus, there is an additional constraint at end of the chain and the radius should approach a constant radius right at the ends of the chain.



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V11.0.2
Function: FEATURE_MODEL

Ref: 002-8000589

KB Article ID# PL8000589

Contents

SummaryDetails

Associated Components

Modeling